STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Using HAL SPI on H3LIS200DL

Hello:Previously using CMSIS, I was able to read or read/write this accelerometer device. Using HAL, I am having some problems. To start, I am trying to read the ID register. I am writing in the address and a dummy byte. The address for the ID regist...

Strange CAN_ID behaviour

I am currently working on a project for a Battery Management System. For this I need to communicate with the rest of a car via CAN. However, my CAN has strange behaviour when sending messages. When I try to send a message at 4Hz (so not fast at all),...

0690X000008BYlbQAG.png
YFric by Associate II
  • 2700 Views
  • 0 replies
  • 0 kudos

Noise problem with ADC

Good morning,I have a problem with the adc converter of the microcontroller stm32L053. I am in the prototype state and am using the Discovery Board.I only have the analog AN0 pin connected to ground. When I execute the reading the converter does not ...

0690X000008BQzUQAW.png

[STM32F407VET6] Is it possible to use the BOOT0 pin as GPIO?

Hi,I'm interested to know what may be happening that STlink can not find the STM32.A strange thing is that the BOOT0 pin is being used as a GPIO. This pin is actuating an opto coupler (it is connected to pin 1 of a PC817)What do I need to ensure for ...

by Not applicable
  • 1158 Views
  • 1 replies
  • 0 kudos

A priority on callback ?

Dear Members,I have two interrupts on my callback,how can I make a priority for them ? Thankscode :void HAL_UART_RxCpltCallback(UART_HandleTypeDef* huart) { if(huart->Instance==USART2) { GPS_CallBack(); } if(huart->Instance==USART1) { ...

STM32F4 DMA Request Mapping Table & TIM1/TIM8 confusion

Using the STM32F446RE with very good results so far including ADC1,ADC2,ADC3 DMA to SRAM arrays. ADCs and DMA (peripheral to memory) were fairly easy but the TIMER 1 and TIMER 8 PWM usage is giving me some problems in understanding how DMA and the ...

0690X000008BUZgQAO.png