STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Can not erase flash memory page using HAL Drivers

Posted on June 18, 2018 at 12:23Hello All.MCU: STM32F031G6U6IDE: System WorkbenchAPI: STM32F0 HAL and low-layer driversI am trying to erase page in the flash memory at address: 0x8002000.Here is the code:https://community.st.com/tags♯/?tags=code‌F...

NUCLEO-H745ZI-Q ADC problems.

Hello everyone!First of all, my apologies if I ask the question wrong or don't provide enough information to start with, I'll of course send all that is needed for better solving of this problem.So, I've gotten the mentioned board and I need to do so...

AMilo.1 by Associate II
  • 2633 Views
  • 5 replies
  • 0 kudos

I'm trying to write and read flash

hi guys, im working on stm32l412kb mcu using keil v5 uvision and i ve found it difficult to write and read flash memory. all the explanation online are not relevant for my mcu. that the way i'm trying to confirm my actions, if anyone understand the p...

Gbasi.1 by Associate II
  • 2179 Views
  • 10 replies
  • 0 kudos

How to deactive XIP in QSPI

Hi, ST example show how to active XIP to read after erase/write data to QSPI. We are success with those step.And, in case we want to change data, we need to deactive XIP. I set command back to Write Directly mode but look like after XIP is enable the...

Dat Tran by Senior II
  • 1381 Views
  • 5 replies
  • 0 kudos

STM32H7 Dual core - power consumption M4 vs M7

Hello,While I was looking for a new MCU, I came across STM32H7 dual core mcus, with M4 and M7.I directly thought that it could be versatile for many usage, M7 for high performance, M4 to mix performances/ and power consumption (and from what I unders...

Rverf.1 by Associate II
  • 5544 Views
  • 5 replies
  • 0 kudos

Address calculation using sizeof() operator

I am a little bit confusing with Address calculation using sizeof() operator.I am writing a program for DMA transfer half a buffer in a time.Such as,---------   1st:      HAL_SPI_Transmit_DMA(&hspi1, ptr1, buf_len/2) ;   2nd:     HAL_SPI_Transmit_DMA...

KAJIK.1 by Associate III
  • 2115 Views
  • 4 replies
  • 0 kudos

Resolved! HRTIM availabilityin STM32G4

Hello all, regarding Application note AN4539 all MCU's of STM32G4 shall support HRTIM peripheral, reference manual also describe HRTIM functionalities for all STM32G4, but on some pages and datasheet it is no information about HRTIM support. Which in...

0690X00000BuetvQAB.png