I am use nucleo-h503rb evk board and i am configure fdcan communication. I have mention below my code please see. I have did not comes output on FDCAN communication.
please send me demo code for that
printf("Initialization complete. Starting main loop.\r\n");/* Configure the FDCAN TX Header */TxHeader.Identifier = 0x321; // Standard or Extended IDTxHeader.DataLength = FDCAN_DLC_BYTES_8; // Data length (up to 64 bytes)TxHeader.BitRateSwitch = FDCA...
also, I Have one of thing just check. I have DSO channel 1 no connected in STM32H503RBT6 board CAN TX pin with respected to ground. But it's not show any output on DSO.