STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

CubeMX Clock Configurator NOT Locking The Selected Values

Hi,in CubeMX clock configuration, after inputting a desired value into one of the PLL outputs (like in the LTDC Clock box) you can lock it and it turns gray (see screenshot), you can then set another related PLL output (like the DSI) and it should re...

Ricko_0-1742744286828.png
Ricko by Senior III
  • 1198 Views
  • 2 replies
  • 0 kudos

STM32G474,HRTIM,ADC

I am using hrtim to trigger the adc, but if the regular channel is not triggered with hrtim, it doesn't go into the interrupt of the ADC properly, I checked a lot of information and didn't find a solution, here is my code and cubemx configuration:   ...

iskan_0-1695029126119.png iskan_2-1695029415264.png iskan_3-1695029424941.png
iskan by Associate III
  • 1843 Views
  • 1 replies
  • 0 kudos

MX cube corrupts .ioc on save (Windows 11)

I am using the STM32CubeMX to edit pinout configurations for the STM32U595ZJYxQ. Process worked well for the past few days however on Friday the tool appeared to hang after saving the config. The first time this happened the tool closed on its own af...

edwal by Associate II
  • 2616 Views
  • 7 replies
  • 1 kudos

How to set SPI_TX in DMA settings

Hi, I’m new to STM32. I wanted to set SPI_TX in DMA settings, but I think it has to be configured before using it, as you can see in the picture. I want to give an output for display... can anyone help to solve the problem?  

AndrewNeil_0-1741705395983.png
Ruvi2006 by Associate
  • 2021 Views
  • 3 replies
  • 0 kudos

Resolved! STM32G030K6T6 - can not configure ADC1_IN16 @ PA12

STM32G030K6T6 - can not configure ADC1_IN16 @ PA12The STM32CubeIDE does not allowed me to enable the ADC1_IN16.The message is "IN16 Disable...Available if sequencer is set to not fully configurable in parameter settings tab"How can I enable it?

GErma.1 by Associate III
  • 3620 Views
  • 4 replies
  • 0 kudos