Hello, after experimenting MEMS sensors with the IKS4A1, I developed a custom board based on STM32F407 CPU with the LSM6DSV16XTR accelerometer+gyroscope and LIS2MDLTR magnetometer.The aim is to get board inclination and compass information with t...
Hello,
on a custom board which mounts STM32F407 CPU with LSM6DSV16XTR accelerometer+gyroscope and LIS2MDLTR magnetometer I have to implement an inclinometer and a eCompass with the maximum accuracy.
Now, it is not completely clear to me how to g...
Hello, I have a custom board with STM32F407 CPU, LSM6DSV16XTR accelerometer+gyroscope and LIS2MDLTR magnetometer.I aim to get board inclination and the position of the north using the magnetometer for a telescope. Using CubeMX, I have enabled th...
Hello, I have a board based on the stepper driver L6472. I noticed that, when I do not provide input 12V for the motor (the motor 12V but I provide the 3.3V for the logic (VREG, VDD, SW), I find a voltage of about 2.6V on the VSA, VSB pins. I tr...
Hello, I am trying to test the e-compass application with the IKS4A1 connected to a Nucleo-F446 and Unicleo-GUI. The firmware of the Nucleo F446 was produced from Cube-MX following the "Getting started with the STMicroelectronics X-CUBE-MEMS1 softwar...
Thank you Andrew you are right, here the link.https://community.st.com/t5/stm32cubemx-mcus/x-cube-mems1-application-inclinometer-and-ecompass/m-p/711271#M29182
OK, fixed by adding the following lines in the provided USE_CODE areas in main.c: extern I2C_HandleTypeDef hi2c1;
BSP_I2C1_Init(); Now it is not completely clear to me how to get the most accurate inclination an eCompass information since there are ...
Thank you Miroslav, set the TIM3 interrupt and increased the stack size, installed MEMS-Studio and now everything is fine. I am very happy. Thank you!!!!
Hello Miroslav, I followed the instructions provided on the document "Getting started with the STMicroelectronics X-CUBE-MEMS1 software package for STM32MX". It is inside the directory \en.x-cube-mems1\Documentation. At page 53 and 60 it is said to s...