STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1670 Views
  • 0 replies
  • 2 kudos

Resolved! Trouble using alternate function on STM32C092

Hi,  i'm missing something in the configuration of alternate function on STM32C092. I can't get working alternare function on shared pin, interested physical pin are  PIN 1, 15, 20.  Example1: PIN15 only the function on PA8 are working properly, neit...

Sanderthunder_0-1762329932926.png Sanderthunder_1-1762330470607.png Sanderthunder_3-1762331610233.png Sanderthunder_2-1762330978487.png

arm_math library source lacks some functions

Hello all, I need to use some FFT functions. I have installed the CMSIS-DSP 1.16.2 and CMSIS 6.3 core as it was required from  CMSIS-DSP. Surprisingly, CubeMX did only a part of its job, namely it did not copy source files and did not add proper incl...

DmitryR by Senior
  • 353 Views
  • 3 replies
  • 0 kudos

Resolved! STM32CubeMX 6.17.0 generated project lost <root folder>

  I have tried using STM32CubeMX 6.17.0 to generate an STM32F429 DISC1 project.The generated project opened in STM32CubeIDE could not be compiled unless I add <root folder> in Project -> Properties -> C/C++ General -> Path and Symbols, the source loc...

NEdom1_0-1776665960643.png
NEdom.1 by Associate III
  • 285 Views
  • 4 replies
  • 0 kudos

STM32CUBEMX rendering bug serious

I am experiencing an issue in STM32CubeMX where all peripheral Configuration panels stay empty, while the Mode panels and System Core → Parameters render correctly.What I have already tried:Starting CubeMX standalone (not via CubeIDE)Creating a compl...

CDekker by Associate
  • 285 Views
  • 3 replies
  • 0 kudos

Resolved! STM32C071FBP6 Pin muxing issue

I am using STM32C071FBP6N MCU TSSOP 20 pin package for one of our project.I am observing Pin_20 is muxed with lot of other pins like PB3/PB4/PB5/PB6. if i select PB3 as GPIO_Output using STM32CubeMx and generated a code. If i try to toggle the pin bu...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.