User Activity

Hello Dear Community,I am working on an HMI System and using STM32H7B0 with APS6404L-3SQR. I am able to do all operations including Write in Memory Mapped Mode but when I try to write 1 byte, It writes 8 bytes which is not what I expect.I have read m...
Hello Dear Community,I am having a real strange issue while using OSPI peripheral in STM32H7B0 custom board.I am trying to use OSPI with PSRAM but I wanna make sure it works fine, so I am using it with a NOR Flash for test.When I try to activate the ...
Hello,There is a typo in Table 14 in page 153. It is mentioned in different places that STM32H7B0 supports OTP but in this table it is not mentioned!Could you please confirm that this variant supports OTP?Thanks,Ayoub  
Hello,I am not sure if this is the right place to report a documentation errors!There is a typo in Table 11 in page 99. The address should be 0x0803 F000  
Hello,I am not sure if this is the right place to report a documentation errors!There is a typo in Table 11 in page 99. The address should be 0x0803 F000