cancel
Showing results for 
Search instead for 
Did you mean: 

Can't open IOC files through file menu; can't save when creating new projects

YouXiaoquan
Associate II

Recently, The CubeMX cannot open IOC files through the file menu, and cannot save IOC files when creating a new project. But I can open the project normally by double clicking an existing IOC file.

Working environment: Win11+CubeMX6.15

I have tried reinstalling CubeMX, lowering CubeMX version to 6.13, and so on, but they all have the same problem.

 

1 ACCEPTED SOLUTION

Accepted Solutions
YouXiaoquan
Associate II

Today, after multiple restarts of the computer, all functions surprisingly returned to normal.

View solution in original post

5 REPLIES 5
Souhaib MAZHOUD
ST Employee

Hello @YouXiaoquan 

Could you please add your IOC file in order to investigate the issue?

BR,

Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

In fact, using the Load Project in the file menu will not bring up a file selection dialog box. And when creating a new project, clicking the save project button will not bring up a save dialog box.

 

Hello @YouXiaoquan 

I am not able to reproduce the issue; I can use the Load Project successfully.

SouhaibMAZHOUD_0-1752588983600.png

Could you start CubeMX using command line and check if there are any errors? 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

This issue is not related to the specific IOC file. Specifically, when using the "Load Project" and "Save Project" menus, CubeMX did not respond.

YouXiaoquan
Associate II

Today, after multiple restarts of the computer, all functions surprisingly returned to normal.