STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1573 Views
  • 0 replies
  • 2 kudos

(STM32CubeMX & Neural-ART ) atonbuf AXISRAM5 raw files

Hello,I'm trying to run a ML model (miniresnet from modelzoo) to a NUCLEO-N627X0-Q starting from STM32CubeMX (initialization of device, model & code generation). Everything is OK when i select STM32Cube.AI MCU runtime, the model is created and runs s...

Unfgr by Associate III
  • 2515 Views
  • 9 replies
  • 3 kudos

Resolved! STM32 Finder missing selectors ?

I would like to filter available products by the following specific peripherals, but those types of filters do not seem to be available.PSSIDMAMUXMDMALPDMAGPDMAHPDMASDRAM support andMinimum #of pins sized package to actually support 1 or 2+ SDRAM chi...

Using Temperature Sensor and VREFINT in STSPIN32G4 MCSDK

Hi , allI am currently working on a project using the STSPIN32G4 together with the STM32 Motor Control SDK (MCSDK). I would like to add the internal Temperature Sensor to monitor the MCU temperature.In STM32CubeMX, I have already enabled both the Tem...

1751018398428.jpg 1751018547608.jpg
1123 by Associate II
  • 1144 Views
  • 0 replies
  • 0 kudos

STM32N6 SPI DMA transfer performance problems

I cant get faster SPI performance, in every SPI DMA request mcu receiving 164 bytes of data, the maximum request rate what I got is about 1KHz, total number of bytes is only ~ 164 * 1000 = 164KB, I need to reach 8KHz rate, MCU and other clocks is set...

TheImmortal_0-1750933721125.png TheImmortal_2-1750933814756.png TheImmortal_1-1750933759715.png

STM32MX as a live peripheral interface

I have a request.The complexity of the peripheral features and the peripheral registers with the inter dependent settings makes it difficult to get everything right the first time or even after multiple tries.  This involves a code generation, code c...

RChap.1 by Associate III
  • 1036 Views
  • 3 replies
  • 2 kudos

Resolved! STM32N6 cubeMX bugs and function portability problems

With new and fast N6 MCU comes new CubeMX package which is full of bugs and errors, I spending hours to find and solve such problems, now I cant trust cubeMX at all, every function must be checked after code generation !ADC rank must be 7, but cubeID...

TheImmortal_0-1750328954613.png TheImmortal_1-1750329528935.png TheImmortal_2-1750330715663.png

STM32H755 Power Regulator Voltage scaling issue

I am using STM32H755 microcontroller and STM32CubeMX V6.14.0 for my development.I am not able to set the clock frequency to 480MHz. Whenever I do so, I receive power regulator voltage scaling error.The product revision used by me is rev.V. The RCC pa...

Damon03_1-1750822248920.png Damon03_2-1750822285264.png
Damon-03 by Associate
  • 780 Views
  • 2 replies
  • 0 kudos