STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1624 Views
  • 0 replies
  • 2 kudos

Resolved! USB and USART1+Flow control simultaneous usage on stm32f107

Translated content. 我在cubemx中同时使能usart1和usb发现有个警告 I enabled usart1 and usb in cubemx and found a warning usart1的流控被usb的dp和dm复用,但是实际上我是没有开流控的 The flow control of usart1 is multiplexed by dp and dm of usb, but I actually didn't turn on the flow contro...

jack_wang_0-1751529668961.png jack_wang_1-1751529715893.png
jack_wang by Associate II
  • 2066 Views
  • 9 replies
  • 2 kudos

Problems configuring a UART

 I'm using the STM32F405RGT6 board in a controller project. I wanted to use PA0 as PWM and PA1 as RX. For some reason, when configuring the .ioc, even though I configure UART4 as receiver only, it doesn't allow me to use PA0 as PWM. Is there any othe...

IMG_0193.jpeg

azure RTOS CMSIS-RTOS2 wrapper for H5

I don't see the wrapper listed in the package for H5 although its listed in this documenten.stm32h5-cube-firmware.pdfwhere can I get it? Is it possible to download and add the package to STM32CubeMX?

Resolved! Partially disabled conflict is hindering CICD pipeline

We are having a similar issue as this person here:https://community.st.com/t5/stm32cubemx-mcus/why-does-the-ioc-file-show-warnings-on-disabled-peripherals/m-p/144500/highlight/true#M5600One of the responses was that this is just a warning message and...

apseftis by Associate II
  • 1108 Views
  • 4 replies
  • 1 kudos