STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1564 Views
  • 0 replies
  • 2 kudos

MX shows Clock Configuration error after updating

I just upgraded STM32CubeIDE from 1.17 to 1.19 which in turn upgraded MX from 6.13 to 6.15Prior to updating, in MX Clock Configuration I could clock the SPI system on the STM32H533 at the same rate as the CPU clock (250 MHz with no error). Now, to av...

Losing GPIO settings

In my project for an STM32H7S3, I have a number of GPIO settings.However, every time I open the file, one particular pin has its settings reverted to the defaults.Also, if I save the IOC file without making any changes at all, I can see in the diff t...

SteveMelnikoff_0-1752583991010.png

STM32H7S78-DR code can't be generated in CubeMX

Hello everybody,I am trying to generate a project for the STM32H7S78 using the latest version of STM32CubeMX. However, when I click on "Generate Code", the process stops at "Copying library files" and does not proceed any further.I usually work with ...

Thinker by Associate
  • 484 Views
  • 1 replies
  • 0 kudos

Invalid SRAM6 Warning for U5A5ZJT6Q

Operating System: Windows 10STM32CubeMX version: 6.10.0STM32CubeU5 Firmware Package V1.4.0 / 20-October-2023When I attempt to validate my X-CUBE-AI model on target, I receive the following pop-up:Exploring STM32CubeMX.log shows the following warning:...

EdgyAI_0-1701470114151.png
EdgyAI by Associate II
  • 2979 Views
  • 3 replies
  • 0 kudos

BUG: CubeMX Code Generation (6.15.0) ST_Cryptolib

Missing pre-processor symbol check in file "Middlewares/ST/ST_Cryptolib/Inc/Commonn/types.h"current line 49:#if !defined(_STDINT_H) && !defined(__stdint_h) && !defined(_STDINT) new line 49:#if !defined(_STDINT_H) && !defined(__stdint_h) && !defined(_...

hga3 by Associate
  • 445 Views
  • 2 replies
  • 1 kudos

RTC_TAMP_IRQHandler Getting continuously triggered.

Hi, I have configured My RTC with LSE of 32.768Khz for STM32G0B1CETxAnd In NVIC Setting RTC & TAMP interrupts are enabled..All these are done using Cube MxAfter HAL_RTC_Init() call from main;  RTC_TAMP_IRQHandler is getting called continuously. Time ...

SPK_FW by Associate II
  • 913 Views
  • 7 replies
  • 1 kudos