cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX Generation error with Eclipse under MacOS

sirin
Associate II

Hello everyone,

I am now using a MacBook Pro with M4Pro chip, running STM32CubeMX 6.13.0 with MacOS Sequoia 15.2 (24C101) Darwin 24.2.0

When SIP (System Integrity Protection) is on, an error of Eclipse occurred each time trying to generate code in STM32CubeMX (I am using STM32H723, if it matters). The message was "The Eclipse executable launcher was unable to locate its companion shared library." And the initial code didn't generated properly. I tried open CubeMX in terminal to see what happens (executing /Applications/STMicroelectronics/STM32CubeMX.app/Contents/MacOs/STM32CubeMX), the log was: 

dlopen(/Applications/STMicroelectronics/STM32CubeMX.app/Contents/Resources/third_parties_plugins/binaries/STM32CubeIDE-MX-services/revA/macosx/cocoa/x86_64/Eclipse.app/Contents/MacOS//../../../../../../pool/plugins/org.eclipse.equinox.launcher.cocoa.macosx.x86_64_1.2.800.v20231003-1442/eclipse_11802.so, 0x0002): tried: '/Applications/STMicroelectronics/STM32CubeMX.app/Contents/Resources/third_parties_plugins/binaries/STM32CubeIDE-MX-services/revA/macosx/cocoa/x86_64/Eclipse.app/Contents/MacOS//../../../../../../pool/plugins/org.eclipse.equinox.launcher.cocoa.macosx.x86_64_1.2.800.v20231003-1442/eclipse_11802.so' (code signature in <66ADAB06-1B30-301C-8ECA-7EDC8C31724D> '/Applications/STMicroelectronics/STM32CubeMX.app/Contents/Resources/third_parties_plugins/binaries/STM32CubeIDE-MX-services/revA/pool/plugins/org.eclipse.equinox.launcher.cocoa.macosx.x86_64_1.2.800.v20231003-1442/eclipse_11802.so' not valid for use in process: mapping process and mapped file (non-platform) have different Team IDs), '/System/Volumes/Preboot/Cryptexes/OS/Applications/STMicroelectronics/STM32CubeMX.app/Contents/Resources/third_parties_plugins/binaries/STM32CubeIDE-MX-services/revA/macosx/cocoa/x86_64/Eclipse.app/Contents/MacOS//../../../../../../pool/plugins/org.eclipse.equinox.launcher.cocoa.macosx.x86_64_1.2.800.v20231003-1442/eclipse_11802.so' (no such file), '/Applications/STMicroelectronics/STM32CubeMX.app/Contents/Resources/third_parties_plugins/binaries/STM32CubeIDE-MX-services/revA/macosx/cocoa/x86_64/Eclipse.app/Contents/MacOS//../../../../../../pool/plugins/org.eclipse.equinox.launcher.cocoa.macosx.x86_64_1.2.800.v20231003-1442/eclipse_11802.so' (code signature in <66ADAB06-1B30-301C-8ECA-7EDC8C31724D> '/Applications/STMicroelectronics/STM32CubeMX.app/Contents/Resources/third_parties_plugins/binaries/STM32CubeIDE-MX-services/revA/pool/plugins/org.eclipse.equinox.launcher.cocoa.macosx.x86_64_1.2.800.v20231003-1442/eclipse_11802.so' not valid for use in process: mapping process and mapped file (non-platform) have different Team IDs), '/Applications/STMicroelectronics/STM32CubeMX.app/Contents/Resources/third_parties_plugins/binaries/STM32CubeIDE-MX-services/revA/pool/plugins/org.eclipse.equinox.launcher.cocoa.macosx.x86_64_1.2.800.v20231003-1442/eclipse_11802.so' (code signature in <66ADAB06-1B30-301C-8ECA-7EDC8C31724D> '/Applications/STMicroelectronics/STM32CubeMX.app/Contents/Resources/third_parties_plugins/binaries/STM32CubeIDE-MX-services/revA/pool/plugins/org.eclipse.equinox.launcher.cocoa.macosx.x86_64_1.2.800.v20231003-1442/eclipse_11802.so' not valid for use in process: mapping process and mapped file (non-platform) have different Team IDs), '/System/Volumes/Preboot/Cryptexes/OS/Applications/STMicroelectronics/STM32CubeMX.app/Contents/Resources/third_parties_plugins/binaries/STM32CubeIDE-MX-services/revA/pool/plugins/org.eclipse.equinox.launcher.cocoa.macosx.x86_64_1.2.800.v20231003-1442/eclipse_11802.so' (no such file), '/Applications/STMicroelectronics/STM32CubeMX.app/Contents/Resources/third_parties_plugins/binaries/STM32CubeIDE-MX-services/revA/pool/plugins/org.eclipse.equinox.launcher.cocoa.macosx.x86_64_1.2.800.v20231003-1442/eclipse_11802.so' (code signature in <66ADAB06-1B30-301C-8ECA-7EDC8C31724D> '/Applications/STMicroelectronics/STM32CubeMX.app/Contents/Resources/third_parties_plugins/binaries/STM32CubeIDE-MX-services/revA/pool/plugins/org.eclipse.equinox.launcher.cocoa.macosx.x86_64_1.2.800.v20231003-1442/eclipse_11802.so' not valid for use in process: mapping process and mapped file (non-platform) have different Team IDs)

(Full log file attached in attachments, the content above may have issues because the forum editor shows 'Your post has been changed because invalid HTML was found in the message body. The invalid HTML has been removed. Please review the message and submit the message when you are satisfied.')

However, when I turned off SIP in RecoveryOS, the STM32CubeMX works well, but I don't want to turn it off regarding safety reasons. I tried re-sign the file that logs mentioned (executing

codesign --force --deep --sign - /path/to/eclipse_11802.so) and it didn't work. Re-installing STM32CubeMX also useless.

And the spctl was disabled (Allowing starting Applications from any source)

I wonder if there's any bug with code of CubeMX or Eclipse? Same problem occurred with my colleague's MacBook.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Souhaib MAZHOUD
ST Employee

Hello @sirin 

This issue has been reported in this thread and it is currently under investigation.

KR,

Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.