STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

Resolved! Clarifications on the Tim1 settings in Cube Mx

I have the following settings in Cube Mx for TIM1The TIM1 is used for PWM generation, but the slave mode, trigger source, clock source are disabled then how Tim1 receives the clock for pwm generation.For TIM4 it is clearly statedSo i assume it will b...

STuser2_0-1754838526230.png STuser2_1-1754838739218.png STuser2_2-1754838838981.png
STuser2 by Senior III
  • 902 Views
  • 5 replies
  • 1 kudos

Missing USER_VECT_TAB_ADDRESS leads to debug issue

I see it's been a while but I ran into this today. Apparently system_stm32g4xx.c that is automatically generated by STM32MX no longer sets SCB->VTOR unless you define USER_VECT_TAB_ADDRESS in that file. When programming that doesn't cause an issue bu...

BobbyBeta by Associate III
  • 619 Views
  • 2 replies
  • 0 kudos

CubeMX and setting analog watchdog

When I try to select which channel gets a watchdog, it only gives me one option on the pull down. Instead, if I want to change the channel, I have to unselect all the ADC channels and make sure that the watchdog intended channel is the first one sele...

AndrewC_0-1754488831788.png
Andrew C by Associate III
  • 614 Views
  • 3 replies
  • 0 kudos

Resolved! STMCubeMX replace the app_freertos.c. How to avoid

I'm developing an app on the demo board STM32U5A9J-DKI've created the project from TouchGFX 4.25.0 project STM32U5A9J-DK FreeRTOSIt perfectly works, compile and debug with both TouchGFX and CubeIDE 1.18.1I then opened the .ioc file of the project wit...

nico23 by Senior III
  • 1713 Views
  • 3 replies
  • 1 kudos