STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

Resolved! Missing Pin PD2 on STM32L433RCTxP

Hey,I´m confused why i can not use Pin PD2 on Cube MX on the Nucleo Board L433RC even though it should actually exist because it exist when you select another STM32L433.Without that Pin, i can´t use SDMMC. If i select for example the STM32L433RCTx, t...

SWend by Associate II
  • 4325 Views
  • 10 replies
  • 0 kudos

STM32L476G-DISCO SPI

Hi,I am working on STM32L476G-DISCO, and I want to interface it with Arduino uisng SPI, but I found that this STM all SPI (SPI1,SPI2 and SPI3) PIN is not on I/O PIN, so how I interface it with Arduino using SPI??

RKhal.2 by Associate III
  • 1280 Views
  • 2 replies
  • 1 kudos

For the STM32F100V8T medium density device can I link TIM2 (master) to TIM15 (slave) using the internal trigger ITR0?

This seems to work fine (timer linkage used in my current firmware) but the Reference manual (Doc ID16188 Rev 5) suggests this internal trigger (ITR0) is not available in low & medium density devices?! Can I rely on all future batches of the STM32F10...

0690X000008A8WtQAK.jpg 0690X000008A8YQQA0.jpg

STM32F401 USB -- USB_CoreReset failed(CSRST bit stucked)

During debugging a bus-powered STM32F401RCT6 customed board, a strange problem was encountered. The application code is directly generated by CubeMX with USB CDC, VBUS sense disabled. The USB failed at plug-in, even no USB enumerating. I tried to deb...

Peerless by Associate II
  • 3780 Views
  • 8 replies
  • 0 kudos

Resolved! Need help downloading STM32Cube_FW_F7_V1.15.0

I am not being able to download STM32Cube_FW_F7_V1.15.0 what so everfrom CubeMx it shows (HTTP access forbidden) errorand when downloading it from browser .. The download always stops at 90% .. trie multiple PCs different times different connections ...