cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX on linux generates a call to arm-none-eabi-objcopy.exe which doesn't exist

Rickta59
Associate

On linux if I use the latest STM32CubeMX (4.26.1) and generate a project for Atollic Truestudio, the project tries to use the executable called 'arm-none-eabi-objcopy.exe' this is the name for the windows verison however on linux it is called 'arm-none-eabi-objcopy' without the extension.

If I fix the project setting and save, the next time I use STM32CubeMX on the same project and regenerate it wipes out my change.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Amel NASRI
ST Employee

Thanks @Rickta59​  for reporting this issue. It will be reviewed by our STM32CubeMX experts.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi Rickta59,

Thanks for your feedback.

I confirm that it is a bug and it will be fixed next release.

Please do not hesitate to contact me for further details.

Thanks and regards,

Mohamed

,

Thanks for your feedback.

I confirm that it is a bug and it will be fixed next release.

Please do not hesitate to contact me for further details.

Thanks and regards,

Mohamed