STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1578 Views
  • 0 replies
  • 2 kudos

CubeMX, mixed C, C++, F767 Nucleo. Getting consistent errors: debugger tries to connect, has following error. Encountered a Socket Error, Exiting..

Getting the following error:code compiles without problem. Code without a certain class compiles and can be downloaded and run. Code *with* class generates following error.STMicroelectronics ST-LINK GDB server. Version 5.1.0Copyright (c) 2018, STMi...

Resolved! USART Communication Nucleo-L4r5zi isn't working?

I'm using the Nucleo-L4r5zi I can't send a receive a simple message using USART Communication, Which pins to configurate on the Cube MX ? should i use an FTDI (usart to usb cable) ?

OGaie by Associate III
  • 1438 Views
  • 1 replies
  • 0 kudos

Atollic true studio CMSIS Description Resource Path Location Type fatal error: arm_math.h: No such file or directory

Hi All,I am using stm32CubeMx and atollic true studio for initializing my stm32H743ZI controller. When I debug the code I get an error message fatal error: arm_math.h: No such file or directory I have tried many things and I am unable to resolve the ...

awais_h by Associate II
  • 1266 Views
  • 1 replies
  • 0 kudos

STM Cube MX vs Matlab simulink, pros and cons

I am a begineer to stm32 it has been two months since I began using STM32 for prototype building. I am currently doing a project which involves DSP. Today I came across an application notes saying we can generate code using matlab too. Now I am confu...

Apill by Senior
  • 2534 Views
  • 6 replies
  • 0 kudos