Browse
STMicroelectronics Community
FAQs
Sign In
Product forums
STM32 MCUs
STM32 MCUs products
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
STM32 MCUs Other solutions
STM32 MPUs
STM32 MPUs products
STM32 MPUs Boards and hardware tools
STM32 MPUs Software development tools
STM32 MPUs Embedded software
STM32 MPUs Solutions
MEMS and sensors
MEMS (sensors)
Imaging (sensors)
Automotive & Transportation
Microcontrollers
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
ZYubi
Associate II
since
2019-02-01
2023-06-14
User statistics
19
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About ZYubi
Options
Report User
User Activity
Posts
Replies
H750VBT6 BKPSRAM can't keep DATA
2019-03-11
/* Enable write access to Backup domain */ PWR->CR1 |= PWR_CR1_DBP; while((PWR->CR1 & PWR_CR1_DBP) == RESET) { } /*Enable BKPRAM clock*/ __HAL_RCC_BKPRAM_CLK_ENABLE(); *(__IO uint32_t*)(0x38800000+36) = 12345678;run to here, DATA 12345678 is writt...
How to get TEMPSENSOR voltage with ADC3 ?
2019-02-21
void ADC3_config(void){ AdcHandle.Instance = ADC3; if (HAL_ADC_DeInit(&AdcHandle) != HAL_OK) { /* ADC de-initialization Error */ //Error_Handler(); } AdcHandle.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4; /* Synchronous clock mode,...
How to read and write 4K BKPSRAM?
2019-02-15
I can't the way in Demo samples.
STM32CUbeMX5.0.1 version can't work well on STM32H750VBT6
2019-02-01
Used to make source code for USB FS Virtual Com, the computer can't connect the device。Same way on STM32F407 chip, it is OK.Is there somebody can help me? Thanks!
Re: STM32F7 - using SPI (slave) with DMA to set a flag (I.E. no interrupts)
2020-02-18
struct { dma_rx[128]; dma_tx[128];} nochache __attribute__ ((aligned (256))); MPU->RBAR = ((uint32_t)&nocache) | MPU_RBAR_VALID_Msk; // using region slot 0 MPU->RASR = MPU_RASR_XN_Msk | // 1: Instruction fetches disabled (3u << MPU_...
Re: STM32F7 - using SPI (slave) with DMA to set a flag (I.E. no interrupts)
2020-02-18
If change the size of dma_rx & tx to 128, How do it?
Re: I can not use backup RAM for STM32H743BI. Is there any application note or source code for backup RAM.
2019-03-11
/* Enable write access to Backup domain */ PWR->CR1 |= PWR_CR1_DBP; while((PWR->CR1 & PWR_CR1_DBP) == RESET) { } /*Enable BKPRAM clock*/ __HAL_RCC_BKPRAM_CLK_ENABLE(); *(__IO uint32_t*)(0x38800000+36) = 12345678;12345678 can be written in BACKUP RA...
Re: I can not use backup RAM for STM32H743BI. Is there any application note or source code for backup RAM.
2019-03-11
I met a problem,The Backup SRAM can read and write,but can't keep DATA when reset the MCU.
Re: H750VBT6 BKPSRAM can't keep DATA
2019-03-11
VBAT is OK. I used the ADC3 to measure the voltage of VBAT, the value is about 3V.
View more