STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1297 Views
  • 0 replies
  • 2 kudos

Resolved! STM32G070CB: STM32CubeMX V5.3.0 with STM32Cube_FW_G0_V1.3.0 fails to configure SYSCLK above 16MHz via the PLL

The following statement inside HAL_InitTick() is not dividing SystemCoreClock by 1000, as it should be. It's dividing by 1. So later, in SysTick_Config(), when argument ticks=64,000,000 which exceeds SysTick_LOAD_RELOAD_Msk of 0xFF'FFFF, a HAL_ERROR ...

DBroo.1 by Associate III
  • 1287 Views
  • 4 replies
  • 0 kudos

SDIO problem when using FatFS on STM32F413

Hi, I am currently working on a project where I will have to log data to an µSD card using a STM32F413. I created a project in STM32CubeMX (version 5.0.0) and setup SDIO (currently in SD 1bit mode, but I also tried 4 bit mode). I also set up FatFS in...

YFric by Associate II
  • 2572 Views
  • 4 replies
  • 0 kudos

Resolved! problem with ADC DMA configuration for STM32H743

I found that STM32Cubemx version 5.3.0 fails to configure ADC DMA operations when building code for the STM32H743.The initialization code set the ConversionDataManagement to the wrong value: hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR...

TBibe by Associate II
  • 3391 Views
  • 3 replies
  • 0 kudos

STM32H757I-EVAL board debug not working in keil ?

Dear All,I had purchased STM32H757I-EVAL board. I am not able successfully debug my program.Events happened in sequence,Successfully booted the demo code. Explored all the function shown on the LCD.Using STMCubeMX (Ver 5.3.0) selected the EVAL board ...