STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

STM32CubeMX 5.2.0 released

Dear communityWe are pleased to announce the release of STM32CubeMX v5.2.0What is new in STM32CubeMX V5.2.0? • Added the support of new dual-core part numbers in the STM32H7 Series: – Added the support of dual-core configuration, code, and project ge...

[Bug report]! stm32f1x ll drivers: function LL_GPIO_Init resets outputs if parameter "pull" isn't assigned, even if the output should be in HIGH mode by default.

To assign pull mode of output pin the function LL_GPIO_SetPinPull writes 0 or 1 to the output buffer (inside the body of LL_GPIO_Init ). Hence if pull-up or pull-down is not necessary (pull parameter equals zero) the output of the pin changes to 0....

Ruslan1 by Associate II
  • 2510 Views
  • 5 replies
  • 0 kudos

Why does code generated from CubeMX not adhere to the C standard?

The C standard says in 7.1.3 Reserved identifiers:"All identifiers that begin with an underscore and either an uppercase letter or another underscore are always reserved for any use."Yet the code CubeMX generates is full of __HAL... identifiers. Is t...

fsch by Associate III
  • 4335 Views
  • 10 replies
  • 0 kudos

Extremly strange bugs (not only one) in actual CubeMx Version

Dear ST,I had an old project from 2017 with Cube and Keil V5 (its not old for Embedded projects). I wanted to change some things but the result was ****. I had freeRTOS configured but this was disabled,.... big troubles. I had already another thread ...

Osto by Senior
  • 1977 Views
  • 4 replies
  • 0 kudos

Resolved! stm32cubemx

Posted on June 26, 2018 at 20:50Hello,I am using the STM32CubeMX application version 4.26.0 (see the attached files)There is no option for me to choose 'Copy all used libraries into the project folder'. The radio button was there but it grey out (di...