cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX project generation have problem BUG on samba

SKape
Associate II

​Hello.

I work on Windows on a network drive.

The file server is samba which, by default, for files whose name starts with a dot, gives the hidden attribute.

After generating the TrueStudio project, the .project and .cproject files are thus given a hidden attribute.

When re-generating the project using CubeMX, the following error appears: '' The Code is fully generated under (mypathname), but TrueSTUDIO project generation have a problem. ''

I can not change file server settings, therefore I am unable to remove the attribute hidden from the .project and .cproject file.

Is it possible the STM32CubeMX will work with the TrueSTUDIO project files that have hidden attributes?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0