STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1565 Views
  • 0 replies
  • 2 kudos

Resolved! STM32L0 PWM TIM with prescaler set to zero, gives no output

I am new to using PWM, so not sure if this is a bug, invalid default settings or wrong documentation.I configured my project using STM32CubeMX.I'm using the internal clock, and the default setting for PRESCALER is 0. I can see in Keil using the debug...

SSkje.1 by Associate II
  • 3581 Views
  • 4 replies
  • 0 kudos

Not reading SPI WHO_AM_I register correctly

Hi everybody,I hope someone there could help me. I am trying to read the WHO_I_AM register of the LIS3MDL magnetic sensor (reg 0x0F). I have a custom pcb with a STM32L151VET6 . I got largley inspired by the STEVAL-WESU-1. I am using STMCubeMx for the...

JMart.5 by Associate II
  • 6455 Views
  • 12 replies
  • 0 kudos

TIM1 OPM mode waveform generation.

i want to generate above signal with variable Toff and Ton fix.i generate code but i don't get my desired out put signal./** ****************************************************************************** * File Name : TIM.c * Descript...

0693W000000UNcIQAW.jpg 0693W000000UNboQAG.jpg

FOTA using STM32

According to AN2606 (STM32 microcontroller system memory boot mode), Section 4.3, we require a 'HOST' peripheral, to communicate with STM32 MCU, in order to get new firmware from the peripheral (while booting from System Memory).Flowchart from Sectio...