STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

STM32CubeMX is not running!

HiI installed STM32CubeMX on my system(Windows 10 OS) but it isn't running!When I try to open it, welcome window pops on but after fading nothing would be opened.I tried to run it as administrator and also I uninstalled and reinstalled it and even re...

STM32 waiting for UART interrupt while doing other tasks

Hello, I am using STM32H7 and Stm32CubeMX. In my current application, I perform a user interface (using UART), and then the system performs a measurement task. However, I need to change the system to perform the user interface and measurement task in...

VYoun by Associate III
  • 3610 Views
  • 5 replies
  • 0 kudos

osKernelStart on STM32 break loop

Hi, I'm use the STM32F429This is my FREERTOSConfig.h#define configUSE_PREEMPTION 1 #define configSUPPORT_STATIC_ALLOCATION 0 #define configSUPPORT_DYNAMIC_ALLOCATION 1 #define configUSE_IDLE_HOOK ...

YiKai by Associate II
  • 1674 Views
  • 1 replies
  • 0 kudos

How to configure SDRAM on 100 pin H7

I am trying to set up the config for a new ST project, but I cannot make the FMC configuration select SDRAM. The tool lets me select the SDRAM mode for different package versions, like the BGA configuration, but not for the 100pin alternative. This h...

DReis.1 by Associate II
  • 4292 Views
  • 8 replies
  • 0 kudos

USB/CDC stops working by adding a asm("nop")

I have some problems with the USB/CDC communication. I have simplified the problem to the following:I'm using STM32CubeIDE and I've used CubeMX to configure a new project with STM32H743IIT6. I set up the clock and the USB/CDC device.The communication...

MRait.14 by Associate II
  • 6105 Views
  • 8 replies
  • 0 kudos

Need help with STM32L476RG SDIO + FATFS project

I have tried communication through SPI by following a lot of youtube tutorials. As there is no ready made library to take care of this through SPI, I decided to give SD mode a try. I am using the STM32L476RG microcontroller that has the SDMMC periphe...

KAbis.1 by Associate II
  • 3776 Views
  • 5 replies
  • 0 kudos