STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1578 Views
  • 0 replies
  • 2 kudos

Resolved! STM32CubeMX BUG:UNINSTALLER DOESN'T RUN

Hi everyone,I wanted to uninstall my STM32CubeMX but uninstaller didn't run. I have downloaded latest version of java.Then I tried to ran uninstaller.jar in cmd I got this error Error: Could not find or load main class com.izforge.izpack.uninstaller....

Onik by Associate II
  • 3912 Views
  • 5 replies
  • 1 kudos

SAI Interface configuration small lack

Hi all,I have noted a lack in CubeMX SAI configuration. When the interface is configured as a Master, it is only possible to set frame length to a power of two from the drop-down list. Despite when I configure it manually to 20 (I need this to implem...

DmRozhd by Associate III
  • 2771 Views
  • 8 replies
  • 0 kudos

Linking error when project resides on UNC path

OS: Windows 10IDE Version: 1.4.0My project resides one a network storage folder, accessable by //BALA/my_project.The network storage is further linked to a virtual storage device, namely B:When trying to compile the project, the linking process retur...

MSonn.1 by Associate
  • 972 Views
  • 0 replies
  • 1 kudos

Resolved! Generic makefile using stm32cubeide

Hi All,How do I generate a generic Makefile from STM32Cube ide? Preferably for L56 series. Currently when I create a project the Makefile option under toolchains inside the cubemx is grayed out. The CubeMX is installed as part of IDE. thanks,

SKuma.14 by Associate
  • 2426 Views
  • 1 replies
  • 0 kudos

Resolved! How to install firmware patch offline

Hello,I have a STM32CubeMX installed on an offline cumputer (that cannot be changed!)I would like to install the last firmware for L0 familly, so I download:stm32cube_fw_l0_v1110.zipstm32cube_fw_l0_v1113.zip (patch only file)From local, there is no p...

ANauz.1 by Senior II
  • 3314 Views
  • 3 replies
  • 1 kudos

Resolved! Any option in CubeMX that allows for changing the stack size of the "Ethif" task ( INTERFACE_THREAD_STACK_SIZE)?

Hello, The stack size is defined by a macro definition, INTERFACE_THREAD_STACK_SIZE inside the "ethernetif.c" file located under: LWIP/Target.I had to manually increase the size due to stack overflow and any new code generation via CubeMX overwrites ...

KSulli by Associate II
  • 4763 Views
  • 7 replies
  • 0 kudos

Flash problem (original STLINK & IC from DigiKey)

I am getting this error, while the setup in cubemx is for this chip... Using SW4STM32.Wrong device detected, check your project and the board(s) connected Open On-Chip Debugger 0.10.0+dev-00021-g524e8c8 (2019-04-12-08:48) Licensed under GNU GPL v2 Fo...

TVan .2 by Associate II
  • 2560 Views
  • 1 replies
  • 0 kudos

Resolved! Issue setting clocks on STM32L412 IDE 1.4.2

Hi,I was playing around a bit with the clocks.I had it set up to run on 48MHz from MSI.I then choose PLL on 64MHz but couldn't get the 1µs timer pulse I wanted (prescaler on 63 for TIM2 got me something about 1,178µs)I then wanted to get back to MSI,...

b.a. by Associate III
  • 1715 Views
  • 4 replies
  • 0 kudos