STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1604 Views
  • 0 replies
  • 2 kudos

No option to set OSR bit in SAI block with CubeMX on STM32H7

I want to use the oversampling feature in SAI block in STM32H742/743/750 device to set MCLK = 512*Ffs (sample frequency).There is the OSR bit in SAI configuration register 1 (SAI_ACR1) to enable this feature. But I cannot configure this feature with ...

AFroi.1 by Associate
  • 815 Views
  • 0 replies
  • 0 kudos

Resolved! X-Cube-SMBUS middleware

Hi,I have downloaded the en.x-cube-smbus.zip package.How can I added it to the stm32CubeIde as a middleware?I have unzipped the file and moved the folder into STM32Cube/Repository/STM32Cube_FW_F3_V1.11.2/Middlewares but it is not seen by the stm32Cub...

lucobos by Associate
  • 2083 Views
  • 2 replies
  • 0 kudos

stm32f746vgt6 sys timebase source tim problem

friends, I have a problem, can you help? I am working with the stm32f746vgt6 microcontroller. I came across something that had never happened to me before. I am using freertos. My crystal frequency is 25 Mhz. Whenever I select the sys timebase source...

0693W000007ZHBEQA4.jpg 0693W000007ZHB4QAO.jpg 0693W000007ZH9wQAG.jpg
mcizmeci by Associate II
  • 4195 Views
  • 7 replies
  • 0 kudos

STM32CubeMX not setting the mcu when generating code.

I have a new pc with STM32CubeMX 6.1.1 and SW4STM32/OpenSTM32 IDE version 2.9.1.I created a simple project setting mcu to STM32L475GTx, activated a few pins and generated code. The project generated has no mcu selected. What is set up incorrectly in ...

PVall by Associate II
  • 4653 Views
  • 6 replies
  • 0 kudos