cancel
Showing results for 
Search instead for 
Did you mean: 

I would like to know if STM32F446VCT7 supports FMC NAND or not.

YDovg.1
Associate II

As far as I read datasheet it says there is a support for that, but in STM32CubeIDE under FMC I cannot select NAND. There is simply no option for that. See attached file.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User

Fixed in rev.8 of 'F446 DS.

JW

View solution in original post

6 REPLIES 6
Uwe Bonnes
Chief

Click NE1 Chis select and you can continue

Actually if I check the NE1 there is no NAND option. Only NOR, RAM or LCD....

So, no I cannot continue...

waclawek.jan
Super User

It appears that there is only one NAND chipselect, NCE3, and that is not present on the 100-pin package. The footnote to Tab.2 in DS10693 Rev 7, mentioning NCE2, is probably copy-paste from the 'F40x datasheet.

@Imen DAHMEN​ , can you please have a look at this issue? Does the 'F446 have FMC_NCE2 or not?

Thanks,

JW

Imen.D
ST Employee

I raised this internally for check and will come back to you with update.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Thanks, Imen.

Jan

waclawek.jan
Super User

Fixed in rev.8 of 'F446 DS.

JW