STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

STMCubeIDE v1.6.1 silent failure generating peripheral files

When configuring TIM peripheral, result tim.c file has something that looks like a java runtime error dump (see attached file around line 110 and later): "FreeMarker template error (DEBUG mode; use RETHROW in production!):"Steps to reproduce this:Con...

JPard.2 by Associate
  • 836 Views
  • 0 replies
  • 0 kudos

Resolved! How to partially configure GPIO using HAL and CubeMX?

Hi,I want to partially configure GPIO's using HAL and CubeMX. In my simple case, I just want to enable/disable the pull-up resistors while running a program.At first I looked up, how the pins get initialized by CubeMX:There's this structure, which yo...

I tried configuring the SAI peripheral in STM32F469. After initialization I was unable to get any clock outputs including MCLK.

Help me in initialization.Here is the initialization i made/* SAI1 init function */void MX_SAI1_Init(void){ /* USER CODE BEGIN SAI1_Init 0 */ /* USER CODE END SAI1_Init 0 */ /* USER CODE BEGIN SAI1_Init 1 */ /* USER CODE END SAI1_Init 1 */ hsai_Block...

SNULU by Associate II
  • 2472 Views
  • 4 replies
  • 0 kudos

what is To Power???

helloI use STM23CubeMX, but i have question.what is To Power???? why to connect system clock to to power??

0693W00000AMRdnQAH.png
MYu.1 by Associate II
  • 2012 Views
  • 4 replies
  • 0 kudos

Resolved! STM32L433 code generation issue

When there is an ADC analog watchdog on DAC1 channel 1 output, cube generates the string ADC_CHANNEL_DAC1CH1_ADC2 (which throws an error) instead of ADC_CHANNEL_DAC1CH1.No big problems but worth telling.

MFran.4 by Senior
  • 1138 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeMX Quick Guide outdated.

I start STM32CUBEMX as beginnger.so I refer to https://www.st.com/content/dam/kms/Contents/Reflibrary/STM32CubeMX_Quick_Guide.pdfbut it outdated. so i want get updated file. also i want to get STM32Programmer reference . ***Moderation Edit: please do...

MYu.1 by Associate II
  • 948 Views
  • 1 replies
  • 0 kudos