cancel
Showing results for 
Search instead for 
Did you mean: 

How to change the CPU in a new project

NW27
Associate III

Hi,

Basically, my new design will use a STM32F767VGT (LQFP100) and I have a NUCLEO-F767ZI development board (STM32F767ZI LQFP144).

All of the ports and functionality I'm using in the new project are available on the development board. I'm using 4 * Uarts, SPI, 2*I2C, SDCARD, USB etc and approximately 20 I/O pins.

I want to develop my STM32MXCube project (ioc file) using the STM32F767VGT and use it to set up all of the ports and name I/O ports as per project function etc etc.

Can I then make a copy of this ioc file and change the processor to the STM32F767ZI LQFP144 for development using the NUCLEO board?

Bringing all hardware configuration across with it?

Thanks,

Neil.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Hi @NW27​ 

You can simply do the import of your project.0693W000004KWUsQAO.pngBest regards,

Nesrine