STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1578 Views
  • 0 replies
  • 2 kudos

Resolved! STM32H745, MDMA_IRQHandler() is missing in stm32h7xx_it.c

I register MDMA call backs, for example XferBufferCpltCallback, XferBlockCpltCallback, etc. using the HAL_MDMA_RegisterCallback() function. But the callbacks never got hit. These callbacks are called from stm32h7xx_hal_mdma.c/HAL_MDMA_IRQHandler(). H...

BVu by Associate III
  • 3003 Views
  • 4 replies
  • 0 kudos

CubeMX deletes existing pin assignments without warning

CubeMX ver 6.2.1 (and also 5.6.1). Start with a new project (STM32G474VE TQFP100 in the attached IOC file). Map pin PC10 to an EXTI function (in my case, falling edge with pull-up) and enable the NVIC EXTI15_10 interrupt. Make sure this pin is "pi...

Bob S by Super User
  • 3059 Views
  • 2 replies
  • 0 kudos

Resolved! STM32G0 HAL upgrade 1.3.0 to 1.4.0

Hello,I updated the HAL libraries for STM32G072RB from 1.3.0 to 1.4.0 (using the CubeIDE and opening the .ioc file and confirming the Migration).However, I can't compile the project any more. Is there something I can do?make -j8 all arm-none-eabi-gc...