STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

I cannot find a program example (HAL_TIM_IC_CaptureCallback() for the input capture mode described in 14.3.6 PWM input mode (13902_STM32_ReferenceManual_11.pdf ). The attached user code works as I expect, but it is unclear to me if everything is correct.

volatile uint32_t udwIC1_Val1 = 0;volatile uint32_t udwIC2_Val1 = 0;volatile uint16_t uwDuty_Cycle = 0;void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef* htim){ if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1) { udwIC1_Val1 = htim->Instance->CCR1; udwI...

0693W00000APLUMQA5.jpg
RGünt.1 by Associate II
  • 1625 Views
  • 2 replies
  • 0 kudos

Inverting UART TX Pin in STM32F103

Hello,I'm porting code from STM32F072 to STM32F103. In F0 I had a option in CubeMX to invert UART Tx pin polarity and it worked very well. I do not have this option in F103's. Is there any way to invert polarity in this uC?BR, Daniel

DKarc by Associate II
  • 5298 Views
  • 2 replies
  • 0 kudos

Nucleo-H753ZI BUG in default configuration

TM32Cube ver 1.6.1 MX ver 6.2.1 with STM32Cube_FW_H7_V1.9.0 - select Nucleo-H753ZI with default configuration and generate new project - add some activity like HAL_GPIO_WritePin(GPIOB, LD3_Pin, GPIO_PIN_SET); HAL_Delay(1000); HAL_GPIO_WritePin(GPIOB,...

mbarg.1 by Lead
  • 2487 Views
  • 6 replies
  • 0 kudos

Which IDE you would choose from STM32CubeMX supported list?

As we know STM32CubeMX support multiple IDEs:STM32 Cube IDEIARKeilI am in midst to decide which one to use. I find this is crucial decision as this would be one used throughout development till production and I don't want to waste time due to toolcha...

BParh.1 by Senior III
  • 2769 Views
  • 2 replies
  • 2 kudos

STM32CubeMX FreeRTOS heap usage estimate incorrect

STM32CubeMX version 6.2.1, target STM3G474VE, CMSIS v2. If you create a time with "static" allocation, the "FreeRTOS Heap Usage" tab shows no heap usage by that timer. However, osTimerNew() always allocates the TimerCallback_t structure from the he...

Bob S by Super User
  • 2993 Views
  • 2 replies
  • 0 kudos