User Activity

Hi allI am having difficulties adding the CMSIS include libraries in the cube IDE, when I attempt to build the project I am getting error messages about files that are already included in the "path and symbols" -> "includes directory". For example th...
Hi STM community,Is anyone here familiar with adding the CMSIS-NN functions in a source code in STM32CubeIDE ?If you are, could you please point me to or provide me with the proper steps to do so ?As I am facing compile error "undefined reference to ...
HiI am trying to include the standard C++ libraries in my STM32CubeIDE code, however I am getting an "Unresolved inclusion" Error. This project is configured as a C++ program, as the project drop down menu only allows me to convert this project to a ...
Hi I am facing issue with the "generate code" to generate the boiler plate code for the nucleo-f44rehere is the software that I am running with :STMCubeMX_v6-0-1Keil ARM-MDK 5.32java version "1.8.0_271" (Java 8 I believe) , which is the recommended v...
Kudos from