STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1570 Views
  • 0 replies
  • 2 kudos

How to correctly configure CubeMx for timer One Pulse Mode?

I am trying to output One Pulse Mode, however the output is not back to 0V when the pulse is complete. The One Pulse is started with a button interrupt.The timing of the One Pulse is correct, but when the pulse is finished, the output was set to high...

0693W00000BctCeQAJ.png 0693W00000BctClQAJ.png 0693W00000BctCqQAJ.png
Xxoyo.1 by Associate III
  • 5206 Views
  • 4 replies
  • 0 kudos

Block diagram of TIM14

Dear All, As you know well STM32CubeMX IDE is showing clock configuration block diagram which is the user programmable interface as showing in the attached picture. My question is ....Can we able to see all the timer block diagrams also in the format...

0693W00000BckoMQAR.png
DLesl by Associate II
  • 1604 Views
  • 3 replies
  • 0 kudos

Resolved! NUCLEO STM32F767ZI: problems to enable USB OTG FS (Host)

I started a STM32 framework project here: https://github.com/FBergemann/STM32-FreeRTOS-Framework/tree/dev-usb-host-msd. And i am currently busy to set up logging to console and USB FS (as Host to USB stick). But i didn't manage to enable USB OTG FS. ...

FBerg.1 by Associate III
  • 5139 Views
  • 10 replies
  • 0 kudos

Out-of-box Cube code generated for STM32F411-E DISCO doesn't run. Error_Handler triggered in clock configuration.

I've just switched to working on an STM32F411-E DIscovery. Starting a new project (STM32CubeIDE) and allowing it to populate the default peripheral config for the board is generating code that will not run (at least not for me).The clock configuratio...

YIzAKat by Associate III
  • 2984 Views
  • 6 replies
  • 0 kudos

Resolved! RTC not changing in Nucleo-F746ZG?

Hi - I have a Nucleo-F746ZG that I am configuring in CubeMX (version 6.2.1). When configuring it I am trying to only set up the RTC and UART3. UART3 is set up to print to the USB virtual COM port (and that works fine).In CubeMX, once I start a new pr...

TMeeh.1 by Associate II
  • 2601 Views
  • 4 replies
  • 0 kudos