STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1545 Views
  • 0 replies
  • 2 kudos

Resolved! STM32CubeMx freeze if DMA Event for SPI4 is activated

Hello,if I generate with CubeMX 6.2.1 (Windows 10 or Ubuntu 20.04) the attached project, it freezes with the following screen:MCU: STM32H7A3V(G-I)Tx2021-07-13 09:20:39,936 [ERROR] runtime:60 - Error executing FreeMarker template FreeMarker template e...

0693W00000BdVm8QAF.png
CKage.1 by Associate
  • 1887 Views
  • 3 replies
  • 0 kudos

Hi, I am using STM32H7A3 board. I need to store a large file. My requirement is to connect an external Flash to STM32 board. When i checked the documents i found QSPI support external flash memory.

The QSPI pins are mentioned in STM32H7A3 reference document. Please refer Img1.In STM32CubeIDE I am seeing the interface as OCTOSPI. Please refer Img2.I need to know Does STM32H7A3 board supports QSPI or OCTOSPI?If it supports , please give the det...

JJoy.1 by Associate III
  • 3173 Views
  • 5 replies
  • 0 kudos

Weird Timer One pulse mode behavior

Hello, I have use Timer 2 in PWM one pulse mode to change the duty cycle of Timer 1 PWM when the pulse have ended using HAL_TIM_PWM_PulseFinishedCallback(TIM_HandleTypeDef *htim)After restart the board, I press the button to trigger Timer2 One Pulse ...

0693W00000BdDq2QAF.png 0693W00000BdDqCQAV.png 0693W00000BdDqMQAV.png 0693W00000BdDqRQAV.png
Xxoyo.1 by Associate III
  • 3085 Views
  • 3 replies
  • 0 kudos

Resolved! SAI Synchronous Slave with BDMA (CubeMX)

Hello All, I am trying to get Full Duplex I2S working with a STM32H7 and a PCM3168A.The STM has 2 SAI blocks (SAI1 A/B) (A in master mode and B in synchronous slave) for sending data to the PCM for the DAC part of the PCM. I use this to transmit 4 Mo...

0693W00000Bd6KOQAZ.png 0693W00000Bd6K9QAJ.png
TCash.1 by Associate III
  • 2912 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H7 QSPI/OSPI critical code-gen bugs (CubeIDE 1.6.1)

Codegeneration for QSPI/OCTOSPI currently fails to enable a required clock and also passes an invalid value in the initialization struct.This is important to fix because especially the clock-issue was very hard to identify (and avoiding such init-pit...

SG.4 by Associate II
  • 2192 Views
  • 3 replies
  • 0 kudos

Resolved! SDMMC 4 Bit wide bus dir voltage converter option

Hello Community,I use the STM32L4R9ZITx and would like to save data on a MicroSD card via SDMMC1. Usually I use the SD 4 bit wide bus mode. After an update of CubeMX and the HAL layers now two more options are offered. One is "Auto Dir Voltage Conver...

0693W00000BdIeuQAF.png
Rookie38 by Associate III
  • 4688 Views
  • 1 replies
  • 1 kudos