User Activity

Hi,To configure my uart baud rate i use a variable on cube MX. To disable error i select "no check" in option --> that work find on previous version.Now with version 6.1.1 the error stay even if i select "no check" with the version 6.1.1.If you have ...
Hi all,On our card with a STM32L4 we use a siliconLabs BGM13P32 for the BLE.The L4 communicate with the BLE SOC in NCP mode (see here for more details). To do that i have integrated the SiliconLabs libs (BGLIB) to our project on stm32cubeIDE.The proj...
Hi, on our card with stm32L496 we have a boot partition that launch the principal application if an update is not required. All work find until i update cubeMX to version 5.6.0 ! Now when i regenerate the code (not changed between the 2 versions) of ...