STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1543 Views
  • 0 replies
  • 2 kudos

Resolved! STM32CubeMX 6.2.1 for NUCLEO-H745ZI-Q doesn't generate PeriphCommonClock_Config() when ADC clocked by PLL3

I create a STM32CubeMx project (test.ioc) for a NUCLEO-H745ZI-Q board and select PPL3 to clock the ADC, but the function PeriphCommonClock_Config() is not generated unless I also clock the USB from PPL3 as well.After enabling a single ADC1 channel I ...

0693W00000Bd2GXQAZ.png 0693W00000Bd2HLQAZ.png
CHossack by Associate III
  • 2765 Views
  • 3 replies
  • 0 kudos

sdcard not working in freertos when using with sdio

Hi all, I have had some problems when working with sdcard (using sdio) in freertos. I use dev kit STM32-E407 Olimex ( it support sdcard slot on board, I use sd card 16GB). when I read sdcard without using freertos, It's working. But when I using free...

TTa.1 by Associate
  • 2234 Views
  • 1 replies
  • 0 kudos

USB CDC CubeMX generated code does not work on STM32F446RE

Hello,I recently started using STM32 Microcontrollers, and before using STM32 Cube IDE, I used Mbed Studio for PC to USB communication using USB, and now having switched to Cube IDE, I can't seem to make the CDC class work, when I try to debug it, it...

MStr.1 by Associate
  • 1126 Views
  • 1 replies
  • 0 kudos
MLync.1 by Associate II
  • 3560 Views
  • 7 replies
  • 0 kudos

Resolved! STM32CubeMx freeze if DMA Event for SPI4 is activated

Hello,if I generate with CubeMX 6.2.1 (Windows 10 or Ubuntu 20.04) the attached project, it freezes with the following screen:MCU: STM32H7A3V(G-I)Tx2021-07-13 09:20:39,936 [ERROR] runtime:60 - Error executing FreeMarker template FreeMarker template e...

0693W00000BdVm8QAF.png
CKage.1 by Associate
  • 1887 Views
  • 3 replies
  • 0 kudos