STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 2 kudos

CubeMX 6.4 doesn't install well on MacOS

Assume for a moment that the target user is a regular person, not someone who knows that applications are stored in /Applications, you have to fire up Terminal, and cd into an app and navigate down to where the the actual programs are kept, and sudo ...

Resolved! CubeIDE 1.8.0 will not open project/.ioc from older version

I have to take an existing CubeMX project and change the micro (F03 -> G03) which should be quite simple, however my CubeIDE refuses to load the project.I can add the project, and it loads all the source files etc. but it will not build (the menu opt...

JU by Senior
  • 1475 Views
  • 3 replies
  • 0 kudos

GPIO A port pins locked on reset

I am facing an issue with GPIOA initialization upon power reset it's LCKR register is set. so I am unable to initialize some of the port pins mode as output.Can any one help me on what would cause it to stay in this state?GPIOA port pins are chosen f...

bvege.1 by Associate
  • 1024 Views
  • 0 replies
  • 0 kudos
Caitlin by Associate
  • 6687 Views
  • 2 replies
  • 2 kudos

Resolved! STM32CubeMX issue for STM32F1 ADC-DMA code

The simple proj is attached to show the wrong code generation for ADC-DMA peripheral.To fix this issue two lines must be changed as below. /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_ADC1_Init(); // ERROR!!! RCC CLK NOT YET ENABLED...

ivainc by Associate III
  • 1036 Views
  • 1 replies
  • 0 kudos