STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1550 Views
  • 0 replies
  • 2 kudos

STM32CubeMX: Feature request - "User Labels" for periphery.

When creating a project with several different hardwares I like the posibility that the CubeMX created definitions for the GPIOs in the main.h header file which can be used in the project and by just changing the project-file one can use a totally di...

stst9180 by Associate III
  • 1260 Views
  • 1 replies
  • 1 kudos

Resolved! STM32Cube code generator bug for STM32G030J6

The generated code has wrong order for MX_DMA_Init() that doesn't work: MX_GPIO_Init(); MX_ADC1_Init(); MX_DMA_Init();...Correct code is: MX_GPIO_Init(); MX_DMA_Init(); MX_ADC1_Init();...note: STM32CubeIDE Version: 1.7.0 Build: 10852_20210715_0634 (U...

Question about STM32H7 clock domains

I am configuring SPI1 on the STM32H743. At first, I used the default configuration where the peripheral is clocked off of PLL1Q as shown below: However, with this configuration, the HAL peripheral driver would time out waiting for EOT flag to be set....

0693W00000JPLOyQAP.png 0693W00000JPLJuQAP.png
JMill.1 by Associate III
  • 2481 Views
  • 3 replies
  • 0 kudos

Resolved! Hello, Today i updated to STM32CubeIDE 1.8.0 However when i tried to create a project based on a B-L4S5I-IOT01A Board i get an error saying

 "Error downloading files: stm32cube_fw_14_v1170.zip (cannot unzipped) and stm32cube_fw_14_v1171.zip (Dependency no loaded). I also tried to update my Firmware using the Help updates links:Check for Embedded package software updates...but i receive t...

BHend.1 by Associate II
  • 3825 Views
  • 9 replies
  • 1 kudos

Resolved! STM32F722RET6 increasing HCLK frequency issue

There is external crystal on my PCB Mfr part: X1E0003410273 I am working on STM32 Cube IDE. At first whenever I enabled external crystal my program did not run at all. Even In low frequencies. Then I enabled Clock Secure System (CSS) Now my program i...

0693W00000JPF4jQAH.png
NChor.1 by Associate II
  • 1616 Views
  • 2 replies
  • 0 kudos

Resolved! Small but serious problem with STM32CubeIDE and STM32CubeMX

When using STM32CubeIDE, it is easy to inadvertantly make changes to source files that are up on the screen, often as a result of the focus being on the wrong window when one types. (This can easily happen when debugging, e.g. I have the focus on a ...

msch by Associate III
  • 3702 Views
  • 8 replies
  • 1 kudos