cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX does not split main.c into individual device files properly - Bug

matt-crc
Senior III

Originally I had the project initialize all devices in main.c.  Since the file was starting to get large, i went to the Code Generator in CubeMX and selected:

mattcrc_0-1741323072344.png

The option to "Keep User Code when re-generating" just doesn't work reliably.  It seems it did not keep the "User Code" for the FMC device, and possibly the RTC device.... I now have to check each and every device manually.

Original FMC init code:

 

 

/* FMC initialization function */
static void MX_FMC_Init(void)
{

  /* USER CODE BEGIN FMC_Init 0 */

  /* USER CODE END FMC_Init 0 */

  FMC_SDRAM_TimingTypeDef SdramTiming = {0};

  /* USER CODE BEGIN FMC_Init 1 */

  /* USER CODE END FMC_Init 1 */

  /** Perform the SDRAM1 memory initialization sequence
  */
  hsdram1.Instance = FMC_SDRAM_DEVICE;
  /* hsdram1.Init */
  hsdram1.Init.SDBank = FMC_SDRAM_BANK1;
  hsdram1.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_9;
  hsdram1.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_13;
  hsdram1.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_32;
  hsdram1.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4;
  hsdram1.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_2;
  hsdram1.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE;
  hsdram1.Init.SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_2;
  hsdram1.Init.ReadBurst = FMC_SDRAM_RBURST_ENABLE;
  hsdram1.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_2;
  /* SdramTiming */
  SdramTiming.LoadToActiveDelay = 2;
  SdramTiming.ExitSelfRefreshDelay = 7;
  SdramTiming.SelfRefreshTime = 5;
  SdramTiming.RowCycleDelay = 6;
  SdramTiming.WriteRecoveryTime = 3;
  SdramTiming.RPDelay = 2;
  SdramTiming.RCDDelay = 2;

  if (HAL_SDRAM_Init(&hsdram1, &SdramTiming) != HAL_OK)
  {
    Error_Handler( );
  }

  /* USER CODE BEGIN FMC_Init 2 */

	FMC_SDRAM_CommandTypeDef Command;
	/* Step 1 and Step 2 already done in HAL_SDRAM_Init() */
	/* Step 3: Configure a clock configuration enable command */
	Command.CommandMode = FMC_SDRAM_CMD_CLK_ENABLE; /* Set MODE bits to "001" */
	Command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK1; /* configure the Target Bank bits */
	Command.AutoRefreshNumber = 1;
	Command.ModeRegisterDefinition = 0;
	if (HAL_SDRAM_SendCommand(&hsdram1, &Command, 0xfff) != HAL_OK) {
		printf("Step 3 error\r\n");
	}
	/* Step 4: Insert 100 us minimum delay - Min HAL Delay is 1ms */
	HAL_Delay(1);
	/* Step 5: Configure a PALL (precharge all) command */
	Command.CommandMode = FMC_SDRAM_CMD_PALL; /* Set MODE bits to "010" */
	if (HAL_SDRAM_SendCommand(&hsdram1, &Command, 0xfff) != HAL_OK) {
		printf("Step 5 error\r\n");
	}
	/* Step 6: Configure an Auto Refresh command */
	Command.CommandMode = FMC_SDRAM_CMD_AUTOREFRESH_MODE; /* Set MODE bits to "011" */
	Command.AutoRefreshNumber = 2;
	if (HAL_SDRAM_SendCommand(&hsdram1, &Command, 0xfff) != HAL_OK) {
		printf("Step 6 error\r\n");
	}
	/* Step 7: Program the external memory mode register */
	Command.CommandMode = FMC_SDRAM_CMD_LOAD_MODE;/*set the MODE bits to "100" */
	Command.ModeRegisterDefinition = (uint32_t) 0 | 0 << 3 | 2 << 4 | 0 << 7
			| 1 << 9;
	if (HAL_SDRAM_SendCommand(&hsdram1, &Command, 0xfff) != HAL_OK) {
		printf("Step 7 error\r\n");
	}
	/* Step 8: Set the refresh rate counter - refer to section SDRAM refresh timer register in RM0455 */
	/* Set the device refresh rate
	 * COUNT = [(SDRAM self refresh time / number of row) x  SDRAM CLK] – 20
	 = [(64ms/4096) * 100MHz] - 20 = 1562.5 - 20 ~ 1542 */
	/* (64ms/8192) * 100MHz) - 20 = 781.25 - 20 = 761 */
	if (HAL_SDRAM_ProgramRefreshRate(&hsdram1, 761) != HAL_OK) {
		printf("Step 8 error\r\n");
	}

  /* USER CODE END FMC_Init 2 */
}

 

 

What CubeMX put in the fmc.c file is:

 

 

/* FMC initialization function */
void MX_FMC_Init(void)
{
  /* USER CODE BEGIN FMC_Init 0 */

  /* USER CODE END FMC_Init 0 */

  FMC_SDRAM_TimingTypeDef SdramTiming = {0};

  /* USER CODE BEGIN FMC_Init 1 */

  /* USER CODE END FMC_Init 1 */

  /** Perform the SDRAM1 memory initialization sequence
  */
  hsdram1.Instance = FMC_SDRAM_DEVICE;
  /* hsdram1.Init */
  hsdram1.Init.SDBank = FMC_SDRAM_BANK1;
  hsdram1.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_9;
  hsdram1.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_13;
  hsdram1.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_32;
  hsdram1.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4;
  hsdram1.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_2;
  hsdram1.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE;
  hsdram1.Init.SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_2;
  hsdram1.Init.ReadBurst = FMC_SDRAM_RBURST_ENABLE;
  hsdram1.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_2;
  /* SdramTiming */
  SdramTiming.LoadToActiveDelay = 2;
  SdramTiming.ExitSelfRefreshDelay = 7;
  SdramTiming.SelfRefreshTime = 5;
  SdramTiming.RowCycleDelay = 6;
  SdramTiming.WriteRecoveryTime = 3;
  SdramTiming.RPDelay = 2;
  SdramTiming.RCDDelay = 2;

  if (HAL_SDRAM_Init(&hsdram1, &SdramTiming) != HAL_OK)
  {
    Error_Handler( );
  }

  /* USER CODE BEGIN FMC_Init 2 */

  /* USER CODE END FMC_Init 2 */
}

 

 

 

Some "User Code" was put in the new files, in other places it just dropped the user code.

 

7 REPLIES 7
Ghofrane GSOURI
ST Employee

Hello @matt-crc 

First let me thank you for posting.

I would appreciate it if you could provide your IOC so that I can further investigate.

I will be waiting for your feedback.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi @Ghofrane GSOURI 

See attached

Hello @matt-crc 

We appreciate you bringing this to our attention.

Issue has been raised to dev team for fix.

Internal number ticket 204844 

THX

Ghofrane

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Andrew Neil
Super User

Just to be clear:

  1. You started a project, generating all the initialisation code in main.c
  2. You changed the project configuration to separate .c/.h files
  3. Your User Code from (1) for the FMC was not transferred into the new .c/.h files

Yes?

If so, was any User Code at all from the original main.c transferred to the new .c/.h files ?

 

Possibly, it's not intended that changing this setting on an existing project should retain previous User Code ?

@Ghofrane GSOURI  ?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

@Andrew Neil 

3 - yes

Was any user code at all from the original main.c transferred to the .c/.h files? - it doesn't look like it.  So far, I had to modify the FMC.c, RTC.c, and SDMMC.c to get back where I was before.  The main.c file maintained the user code that was not part of the peripheral initialization and deleted everything else.

I understand what you are saying, but...

a) the same "user code" comment areas exist in the new files as well as the original main.c 

b) if it was not intended to transfer the code to the new files (by design), then there should have been a warning in the GUI, because it was not obvious to me.


@matt-crc wrote:

b) if it was not intended to transfer the code to the new files (by design), then there should have been a warning in the GUI, because it was not obvious to me.


Absolutely.

So, @Ghofrane GSOURI the question is whether this is the intended behaviour? If it is, then it needs to be made clear!

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User

Another one with the same issue - specifically related to TouchGFX:

https://community.st.com/t5/stm32cubemx-mcus/bug-or-ill-advised-design-choice-converting-between-pairs-of-c-h/m-p/793305

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.