STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1559 Views
  • 0 replies
  • 2 kudos

I was wondering where STM stand with RUST language?

I was wondering where STM stands with RUST language. I see no website within st.com about RUST support.Is there a plan to add RUST into STM32 CubeMX and STM32-IDE as native support, if so, what kind of timescale that it appears?Will FreeRTOS and Azur...

Riscy by Senior
  • 2813 Views
  • 1 replies
  • 1 kudos

Software Packs (ALL) option missing for STM32CubeMX

Hello every one ,i'm a chinese student.Recently,i installed CubeMX again (i have ever installed it oneyear ago).And i fond this problem again.The Software Packs is unvisible in CubeMX.Also,i searched this problem in chinese BBS,and i cant see a same ...

0693W00000Y8qVjQAJ.jpg 0693W00000Y8qVwQAJ.jpg
ChenKai by Associate
  • 1979 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeMX Linker script generation problem

Hello,I noticed that when I create new project in STM32CubeMX 6.7.0 (STM32F030F4Px) and set "Minimum Heap Size" to 0x0 and "Minimum Stack Size" to 0x0, the linker script is not generated (project with default settings, I only change "Toolchain / IDE"...

pawcuq by Associate II
  • 6261 Views
  • 6 replies
  • 0 kudos

struggles with output compare mode one pulse --- stm32l476rg?

Hello...I am struggling (for a week now) trying to figure out how this output compare stuff works....Documentation is very poor on this and naming conventions are all over the place....I would like to gate timer15 with a pulse from timer1. I am expe...

0693W00000Y8gznQAB.png
SWenn.1 by Senior III
  • 1826 Views
  • 3 replies
  • 0 kudos

Resolved! STM32U5 ADC hangs at calibration

I have a nucleo-U575ZI-Q and can run the examples for the ADCs just fine. However when I try and make my own project using STM32CubeMX the code hangs at the ADC calibration. I've gone over the settings a dozen times and compared them against the ex...

ASimo.3 by Associate III
  • 4556 Views
  • 2 replies
  • 2 kudos

Resolved! How to send and receive UDP packets on the Nucleo-H723ZG board?

I am trying to use LWIP on the STM32H723 Nucleo board to send and receive UDP packets. I have generated code using CubeMX version 6.70 and configured it to use LWIP with FreeRTOS. I have referred to the H7 series LWIP related problems and H723 addres...

Daecheol by Associate II
  • 6470 Views
  • 3 replies
  • 0 kudos

Unable to use USB-OTG on NUCLEO-H755ZI-Q with CubeMX 6.7.0

I'm trying to use USB-OTG on NUCLEO-H755ZI-Q. I first created a new project within STM32CubeIDE and set all pins to their default setting. Then, I set USB-OTG to CDC and downloaded it to my board.​However, with CubeMX 6.7.0, I can not see the USB dev...

0693W00000Y8UjmQAF.png 0693W00000Y8UjhQAF.png
TKuo.1 by Associate III
  • 2844 Views
  • 5 replies
  • 0 kudos

Resolved! ETH LWIP with RTOS | bug in ethernetif.c: HAL_ETH_Start_IT

SetupSTM32CubeIde 1.10.1STM32CubeMX 6.6.1.202207061420RegardingSTM32F4/F7/H7 projects (maybe also exends to others) with Ethernet, LwIP and RTOS features activated.Especially when the WITH_RTOS flag is set in LwIP>General settings.SymptomsEthernet li...

PeterH by Associate II
  • 2554 Views
  • 2 replies
  • 1 kudos