STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1628 Views
  • 0 replies
  • 2 kudos

Lockup in I2C driver with STM32Cube_FW_H7_V1.11.0

This is more of a notice than a question.I just spend the past week looking into an issue we had with reads from an I2C connected EEPROM. We noticed that our system started hanging after some time; sometimes after over 5h.After a lot of searching we ...

Arno1 by Senior
  • 5619 Views
  • 9 replies
  • 1 kudos

STM32 USB HS DMA stuck

Hello.I try to setup CDC USB HS with DMA but it blocks after few samples sent.Here is the minimal code that replicate the problemint main(void) { /* USER CODE BEGIN 1 */   /* USER CODE END 1 */   /* MCU Configuration----------------------------...

0693W00000UnWheQAF.png 0693W00000UnWhtQAF.png 0693W00000UnWjpQAF.png 0693W00000UnWirQAF.png
VSerb.1 by Associate
  • 2194 Views
  • 2 replies
  • 0 kudos

CubeMX define "USE_HAL_USART_REGISTER_CALLBACKS"

Hello,The CubeMX and the ST HAL has in the files "stm32XXxx_hal_conf.h" the#define USE_HAL_USART_REGISTER_CALLBACKSWhen I looking in the source code, there is no position to find where is this define used:Searching for 'USE_HAL_USART_REGISTER_CALLBAC...

_legacyfs_online_stmicro_images_0693W00000biiOIQAY.png
MMüll.6 by Associate III
  • 2036 Views
  • 3 replies
  • 0 kudos

Resolved! Flashing empty memory pages with cubemx locks my mcu

Good evening stm32 dwellings, i have a flash problem.I find myself with the need to write a config file independent to my programm code.In order to do that my programm uses pointers to specific memory pages of my stm32f105:define ADDR_FLASH_PAGE_54 ...

0693W000007EwP0QAK.png
Javier1 by Principal
  • 2622 Views
  • 2 replies
  • 1 kudos

I have most recent version STM32CubeMX, but it keeps popping up do you want to generate code every few minutes, it is annoying. I prefer to generate code when I exit the CubeMX, how to restore that configfuration?

I have most recent version STM32CubeMX, but it keeps popping up do you want to generate code every few minutes, it is annoying. I prefer to generate code when I exit the CubeMX, how to restore that configfuration?

Occasional Data Corruption in the external SDRAM in STM32F429

Hi,I run an application with stm32f429zg using freertos. An external 8Mb SDRAM from winbond (W9864G6KH-6) is used with fmc protocol. I set timing settings in stm32cubemx based on the sdram datasheet.The common clock of sdram is 72Mhz. All other setti...

0693W00000bhPdvQAE.png
MZoli.1 by Associate II
  • 2184 Views
  • 2 replies
  • 0 kudos

Installation issues...maybe?

This is more of a Linux issue, I think, than an IDE or MX issue. I've installed the latest versions of these applications and, unlike the previous installations, I'm not having the .ioc and .project/cproject files recognized as IDE/MX applications a...

TJM by Senior II
  • 1873 Views
  • 3 replies
  • 0 kudos