I was given an example that was created with version 6.6.1. I upgraded to from 6.6.0 to 6.6.1 and the system still thinks I am using 6.6.0. How do I fix this?
Failed to copy file:C:\TouchGFXProjects\P51NG\CM7\TouchGFX\assets\images\gauge01_needle.png to C:\TouchGFXProjects\P51NG\CM7\TouchGFX\assets\imagessee log for more information
Here is more information on the issue. when I am doing a compile with the ioc file I get a message that I have not configured the Platform Settings correctly, but I cannot configure the settings. That might me my problem.
Yes I can erase each block except the block that I was programming in. It is the first block on the 0x90000000 external flash. I cannot seem to erase it with the stm32cubeprogrammer. I get and error.
Sorry my question was too general. I started TouchGFX 4.18.0. Created a project from the template for STM32H745I-Disco. Added a box, made it blue. Added a button with text and compiled it.I could not get it to download with this basic setup to the ta...