User Activity

Hi. Is it possible to generate code with CubeMX for multiple configurations, which can be initialized on-the-fly?Example: I have only one UART available, e.g. UART1, which can be connecrted directly via RS232 voltage translator, or when USB VBUS volt...
I am trying to start HSE with external crystal (on nucleo WL55JC1 board). I removed R2 (Output from TCXO), added two 0E bridges R39 and R40, added 10k resistor R41 (to remove stub). Then I started the Cube-MX (latest, fresh update...), selected the n...
Posted on February 24, 2016 at 08:27I have several discovery boards and last week I got a nucleo board. I made a mistake and connected another SWD debugger to STM32F103 SWD pins instead of on-board target microcontroller and erased ST-Link firmware....
Posted on June 15, 2011 at 15:16Few modifications are required, but it's easy to connect. I prepared brief instructions how to connect ULINK2 to Discovery board:http://e.pavlin.si/2011/06/14/stm32l-discovery-and-ulink2/Marko #ulink2 #st-link #uli...