STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1538 Views
  • 0 replies
  • 2 kudos

Resolved! Cubemx & Stm32U031

Inside Cube config, i do not get the other internal connected pins on pin 14, only PA8... in older versions it was available. The chip is STM32U031F8... What do i do wrong.. i need to use the uart_tx function on pin 14... Thank you  Old version from ...

KJeps3_0-1771255803170.jpeg KJeps3_1-1771255810598.jpeg
KJeps.3 by Associate III
  • 367 Views
  • 5 replies
  • 1 kudos

Resolved! STM32CubeMX generated USBPD not compiling

Hello, I created a complex project for a STM32H573 based custom board. That project is ThreadX based and it shall use the USPBD package. I generated to project with STM32CubeMX version 6.16.1 using STM32Cube MCU Package for STM32H5 Series 1.5.1 (see ...

TThan by Associate III
  • 438 Views
  • 4 replies
  • 3 kudos

Where to report bugs?

I've reported a STM32CubeMX bug, but I am afraid that there is no one to look at it. Is there any better place to report bugs/issues? Things I've reported are quite a blocker for me and I really need to know if there is anyone working on it, or I'll ...

Resolved! Can CubeMX generate a cpp file

I'm using "STM32CubeIDE for Visual Studio Code" on Ubuntu 22.04.  I have a situation where I'm making a driver for a chip where it very much benefits me to make the driver into a class and instantiate several instances of it.Generally speaking, what ...

sethkaz by Associate III
  • 343 Views
  • 2 replies
  • 3 kudos