STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

About STM32F429IGTx clock setting

Hello, I would like to ask about the clock configuration of STM32F429.I use STMcubeIDE for project configuration and my clock configuration is as follows:  The GPIO port is configured as follows: I tried to turn on an LED light, but the program froze...

屏幕截图 2023-07-20 001432.png 2FQU4VGI8@O$(%9%XJG{$3I.png
ZYL by Associate
  • 1475 Views
  • 1 replies
  • 0 kudos

Resolved! BUG: CubeMX FreeRTOS projects corrupt memory

Typical user symptom: sprintf with floating point doesn't work or crashes.I've provided a complete explanation and required fixes here:http://www.nadler.com/embedded/newlibAndFreeRTOS.htmlTo illustrate the crash in minimal test application, I've prov...

STM32H757 ETH and LCD performance issue

Hi,I am trying to integrate ETH & TFT LCD i nto my application using STm32H757 MCUTFT LCD display interface is working properly unless ETH is configured ETH is configured through below linkhttps://community.st.com/s/article/How-to-create-project-for-...

NAham.1 by Associate II
  • 1501 Views
  • 1 replies
  • 0 kudos

STM32- Can not initialize eMMC, CMDTIMEOUT

I have problem with using stm32 drivers for connection to eMMC.https://datasheet.lcsc.com/lcsc/2205071500_Zetta-ZDEMMC04GA_C3010207.pdfProblem is that the initialization pop up error, because timeout occures in function static uint32_t SDMMC_GetCmdEr...

Trahery by Associate
  • 2514 Views
  • 1 replies
  • 0 kudos

Running STM32CubeMX in command-line mode

Hi,I am trying to generate my project from CubeMX from the command line. If i do this from the standalone STM32CubeMX installation (version 6.6.1) then all works as expected. I am using the instructions from UM1718 section 3,3.2, and running from the...

SCrum.1 by Associate III
  • 2100 Views
  • 1 replies
  • 1 kudos