User Activity

Hello,I am trying to build a BLDC controller using STM32F4. I made a board with the 6 mosfet and drivers, current sensing, Hall sensors input...Is there a ST library for motor control ? I found differents tools (MC workbench), but they seems to be de...
Hello,I try to synchronise 6 PWM outputs for an BLDC controller.I use 3 timers :My target is STM32F446RET6 and I'm using STM32CubeIDE.I read that I add to use master/slave mode. I'm not sure it is the best way, but I configured TIM2 (slave) as follow...
Hello,I created a BLE peripheral using a BlueNRG-MS chip. I can connect on this peripheral using a BlueNRG-M2 (using BlueNRG GUI) and read the services.However, it does not work when I try to connect with an android device (I use "BLE Scanner" app, B...
Hello,I'm trying to follow the test procedure for BlueNRG-MS (SPI) indicated in the Bringing up the BlueNRG and BlueNRG-MS devices - Application note (AN4494).I'm using an STEVAL-IDB005V1D board (with a BLUENRG-MS chip) and an NUCLEO-F446RE board to ...
Hello,I bought an STEVAL-IDB005V1D board with an BlueNRG-MS chip. Is it possible to control the chip with BlueNRG GUI through the SPI of the STLINK-V3SET ?I could do it for a BlueNRG-M2 board through UART, but it does not seem to work with the BlueNR...