User Activity

Hi there,is there a possibility in CubeMX to add a remark/comment/note to a peripheral or its configuration?Background:I would like to leave a note (in CubeMX) about what I use Timer5 for and why I configured it that way 
Hi,I'm using CubeIDE: V1.10.1 (CubeMX v6.6.1).To configure my project in (internal) CubeMX, I have created a "user constant":Name: USER_01Value: 7In FreeFRTOS Config parameters -> LIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY,I have entered this "USER_01" W...
I want to use the OSC32_OUT Pin (PC15) of the STM32L432KC as general purpose output. Moreover i connected a FET with a pullup to this pin and want to control them. I do not use any LSE oscillator functionality. The datasheet states that upon reset th...
I want to use the bootloader feature (via UART) of the STM32L071RB. I have read the AN2606 and AN3155.If I'm right, the STM32L071RB has a V11.x bootloader and can be updated via UARTx, SPIx,and I2Cx.Is is possible to configure, which pins are used by...