STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1637 Views
  • 0 replies
  • 2 kudos

CubeMX FMC Import Errors

HiSee attached IOC.  When I import this to a clean (just created in CubeMX, version shown in attached) project the FMC is, incorrectly, flagged as having errors.  I do not know if other aspects are imported correctly or not.Method:start CubeMXFile > ...

MRobe.1 by Associate III
  • 1418 Views
  • 0 replies
  • 1 kudos

IOC Migrate Issue, Project Structure

HiWhen I create a new project (STM32F429NIH) and use an old file which I migrate to the latest IOC format I find that I must go in and edit it: ProjectManager.MainLocation=SrcProjectManager.ProjectStructure=ProjectManager.ProjectFileName=STCubeGenera...

MRobe.1 by Associate III
  • 1035 Views
  • 0 replies
  • 0 kudos

CubeMX: accidentally disabled TIM6

While enabling Timers in CubeMX, I accidentally clicked on TIM6 which is already on by default and used by the Core I believe. I re-enabled it by clicking on it again and of course the default settings got erased. And now whenever I try to run my cod...

TIM6.PNG TargetError.PNG

UART DMA race condition bug

Hi, I want to discuss this problem in UART DMA on STM32F4 boardsI am sorry to upload picture rather than code.Moreover, my English is not proficient and please understand.I tested my code under nucleo-f429zi.------------------------------------------...

Taehyun9203_0-1693113902193.png Taehyun9203_4-1693114628194.png Taehyun9203_5-1693114892969.png Taehyun9203_6-1693115098198.png

Resolved! NUCLEO-H723ZG LSE option is grayed out in CUBE MX version 6.9.1

Hello,I'm in Cube MX and trying to activate the LSE option of my NUCLEO-H723ZG but the option is not available. I see many others which are notavailable.Why? I see that the external low frequency oscillator is correctly installed into the board...Che...

FCamp.1 by Associate III
  • 1913 Views
  • 2 replies
  • 2 kudos

Selecting HSE as clock gives error

Hello, I have a problem trying to create a project in STM32CubeMX with a custom board using STM32L476RGT6 with crystal oscillator of 32MHz. In the interface configuration, when I selected HSE and set the value of 32MHz, it failed to initialize the pe...

User2501 by Associate II
  • 2102 Views
  • 3 replies
  • 0 kudos