User Activity

Dear ST,I was not able to find any documentation for composite builder feature of your USB MW library. Is it documented somewhere?I was able to get USB composite device running after enabling USE_USBD_COMPOSITE define. But I had to fix some bugs, tha...
I've created a project using STM32H7B3I-DK eval board with all settings default, unmodified, taken from TouchGFX. UI menu is working fine with some resources stored in OSPI Flash memory.Now I wish to store some data in this OSPI memory. The procedure...
I've created a project using STM32H7B3I-DK eval board with all settings default, unmodified, taken from TouchGFX. UI menu is working fine with some resources stored in OSPI Flash memory.Now I wish to store some data in this OSPI memory. The procedure...
I'm trying to create new project with STM32H7B3I-DK and the following error is reporter. Designer version 4.15.0Log file contents from today:2020-11-24 22:44:30,981 [1] INFO TouchGFXDesigner.App: Logging configured2020-11-24 22:44:32,251 [1] INFO Tou...
Kudos from