STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1628 Views
  • 0 replies
  • 2 kudos

Configure STM32 U585 UART in single-wire half duplex mode

I am trying to configure the LPUART1 on STM32U585 in single-wire half duplex mode. As I understand, in half-duplex mode, only one pin is configured which is used to send and receive data. I need the half-duplex mode for self-test in my code letting m...

Neharika by Associate II
  • 5738 Views
  • 6 replies
  • 0 kudos

Resolved! CubeMX 6.10.0 has wrong SRAM size for STM32L452

I migrated a project from STM32CubeMX 6.3.0 to STM32CubeMX 6.10.0.  It didn't boot anymore.There was this interesting diff to the linker script: ** Abstract : Linker script for STM32L452VCIx series -** 256Kbytes FLASH and 160Kbytes...

tpiepho by Associate
  • 2779 Views
  • 4 replies
  • 2 kudos

I can't install STM32CubeMX on Mac with M2 core

When I try to install the application, it opens and closes and does not give any errors. I read the readme.html file but the ones there did not work. Can you give some information about how I should install it?

0693W00000aJLmcQAG.png
efebasol by Associate
  • 2994 Views
  • 4 replies
  • 1 kudos

Resolved! Setting 38400 baud rate reception with SPI

Need to achieve 38400 baud rate for reception of NMEA messages but here 38400 is not in the multiple of binary numbers.Setting the clock to 8MHz and then using prescaler is just setting it to 31.25 Kb.How to adjust to be able to achieve that baud rat...

rohan_m_0-1707383007686.png
rohan_m by Senior
  • 3334 Views
  • 3 replies
  • 2 kudos

Resolved! How to change MCU in STM32CubeMX?

Hello,I tried to change the board in my project from STM32G474CC to STM32G473CC. Both should be pin compatible. I've read different solutions for this in the forum but non of them work. Also the description in UM1718 chapter 11.9. When I follow the s...

DMala.2 by Associate
  • 13205 Views
  • 5 replies
  • 2 kudos

Bug: Wrong SAI SPDIF Tx bit clock rate

MCU: STM32F446VESTM32CubeIDE 1.7.0 with CubeMX 6.3.0SAI1 block A is configured in SPDIF TX mode, clock audio frequency is set to 44.1KHz.SAI Clock is approximately 2.823529 MHz. HSE freq is 12MHz.As you can see on screenshot "Real Audio Frequency" al...

sintech by Associate
  • 2858 Views
  • 1 replies
  • 1 kudos

Resolved! HRTIM-E1 Interrupt not firing

HRTIMe1 Interrupt needs HRTIM-MASTER Interrupt to fire?I saw similar issue in GitHub but it pertains to Source of fault.Anyway, I am using STM32G4 V1.3 on STMcubeIDE V1.5.1 on win10 machines (2 PCs)It seems that HRTIM-E1 will not fire up the interrup...

0693W000007B3DhQAK.png 0693W000007B3E1QAK.png 0693W000007B3MFQA0.png 0693W000007B3PnQAK.jpg

Motor Pilot

Dear Team, I am using SPC58 MCU. Can we use motor pilot tool as a addon so that I can integrate this tools with other IDE's. Thanks in advance