Issue resolved. Vector table =)USER_VECT_TAB_ADDRESS. just why system_stm32f4xx.c decided to do it this way, this is starting from the 1.26 package. And the same file on 407 works ok.I laughed for a long time after I solved the problem, I think I'll ...
Thank you. For not passing by =) It's nice when people are not indifferent.Debugged 100 times =)With a debugger, the code goes through the steps every time, so it’s not very clear what the chip doesn’t like. I will search =)Does it make sense to writ...
from the periphery only GPIO. the SFTRSTF flag is constantly raised.But a few lines on CMSIS work fine. after CUBE_MX, a permanent SFTRSTF. :sleepy_face:
board STM32F429I-DISCO MB1075 B-01.The demo example works great. When generating a project in the CUBE_MX 6.8.0,pack 1.27.1 , a soft reset is raised cycle.I do not know what to do