User Activity

A Beginner's inquiry please be patient Local host error in the debugger configuration, ID of both boards ( STMH743ZI2 ) and the updated firmware verified in the " help" update .. Could it be that the " canned " local host " from the download files is...
Yes it is a common problem - just can't find  the problem  -  Download  FDCAN  Files from Youtube controllers site.Software side -IDE,MX  files  okay  except when I get to debug configuration - Error" nost link "   drivers exist in Device Manager  ; ...
AS  in the  TUTORIAL  FDCAN NORMAL OPERATING MODE , What pin on the NUCLEO H743ZI2 -144 board  receives the VVD  ( and  VIO ) from the Transceiver MCP2526FD 8DIP  see attached  Is it a plug in or do I need to create a contact pt . 
Not sure this is the right label Is there  a link  where I can obtain the complete program code for STM32 FDCAN in NORMAL MODE for the STM32H745I-DISCO ( Tutorial ) similar to the entire code MULTI Can .zip  that was found i the link for the STM32 Ca...
The  tutorial and transcript for STM32 FD CAN  LOOPBACK MODE provide  the partial code . Is there the entire code that I can download similar to that found for    TUT_CAN_LOOPBACK code (link) in the STM32 CAN Loopback tutorial  
Kudos from
Kudos given to